Oscillators are used in timing, and are comprised of a resonator circuit and a driver
circuit that detects and amplifies the resonant signal used for timing. The resonator is
usually a mechanical or piezoelectric device made of crystal, ceramic, or an integrated
MEMS (micro-mechanical) structure with resonating properties.
A crystal oscillator circuit is the one of the simplest external timing solutions to
implement. The resonating device is built using a piezoelectric material, commonly
quartz, sandwiched between two metal plates. The crystal (quartz or ceramic) translates
the mechanical resonance vibration into an electrical signal at a set frequency. There
are crystals that can produce pulses ranging in frequency from a few kilohertz to
hundreds of megahertz. Crystals are two-terminal devices that rely on additional
circuitry such as a capacitor in parallel to get the crystal to generate a set
frequency. The circuitry can be located in a microcontroller chip, or the crystal can be
integrated with driver circuitry into a module or chip package.
With respect to different applications, there are different types of oscillators:
Standard clock oscillators typically offer a single frequency that is set at the
factory. Also referred to as simple packaged crystal oscillators (SPXO), these are
the most basic oscillators that combine a quartz crystal with an oscillating
circuit. Applications: <100MHz - replacements, consumer electronics. >100MHz
– SONET/SDH, 10GB Ethernet, Fibre channel.
Programmable oscillators are integrated chip oscillators offering commonly used
reference clocks. The desired clock frequency is typically configured via pin
selection as directed in the datasheet.
TCXO (also TCO) stands for “temperature compensated crystal
oscillator;” is a highly stable combination of a crystal oscillator with a
temperature-compensated circuit. TCXO is excellent for applications requiring
precision timing. Often used for RF applications such as tactical radios, wireless
devices, small cell access applications and nearly all smartphones.
TCVCXO stands for “temperature compensated voltage controlled crystal
oscillator.” This is a crystal oscillator solution that is both temperature
compensated and frequency-controlled via voltage. (Also abbreviated as VCTCXO, or
VC/TCXO) Due to its precision and variable frequency control aspects, applications
include cell and cordless phones, mobile and radio communication equipment.
VCSO stands for “SAW Voltage Controlled Oscillators.” VCSO are used for
applications requiring low jitter and low noise at fundamental frequencies up to
1GHz. On the down-side, VCSOs have very low vibration sensitivity such that their
frequency changes with physical vibration; but this problem is deterministic, or
predictable, such that it may be compensated for. The rugged VCSO is used in various
commercial, telecomm, and military applications.
VCXO (also VCO) is a voltage-controlled crystal oscillator; an oscillator whose
frequency is tuned via a variable voltage input. This offers the option of a stable
crystal oscillator with the ability to fine-tune the frequency within a finite
range. These are often used in industrial equipment, communication relays, digital
TV, digital audio, set top boxes and many other applications.
OCXO is an “oven controlled crystal oscillator,” and is the most
precise and frequency-stable solution available. The quartz crystal, with a zero
temperature gradient at high temperatures, operates in a miniature temperature
controlled environment and is available in surface mount packages measured by the
millimeter. OCXOs find applications in base stations for mobile phones, broadcasting
equipment, navigation system and clock frequency standard, radar, and test &
measuring instruments.
In addition to piezoelectric devices such as crystal or ceramic resonators, there is
a newer addition to this fundamental basis for timing technology. A MEMS resonator
is a small structure (0.1mm or less) that is designed to vibrate at high frequencies
under electrostatic excitation. For precision timing applications, MEMS oscillators
often include temperature compensation by using an on-chip temperature sensor. MEMS
oscillators have superior resistance to shock, are thin, and are well-suited to
co-fabrication in CMOS integration.
Quartz, ceramic and MEMS resonators are one option for the resonating device in a
timing circuit. Another low-cost timing option is a simple RC oscillator, which uses
a resistor and a capacitor with an amplifier to produce an oscillating signal using
positive feedback. Most common output signal is either a sine wave, a
CMOS-compatible output, a TTL-compatible output, or an ECL-compatible output.
However, for precision applications, the traditional solution has been a circuit
based on a vibrating resonator. Crystals and ceramic resonators have well-known
oscillating properties. MEMS resonators are micro-mechanical and are inherently
integrated, resulting in a much smaller footprint, but worse noise performance than
quartz. Quartz has a temperature dependency that is almost zero, whereas a MEMS
oscillator (if etched in silicon) significant temperature dependency and must be
compensated with additional circuitry. Nevertheless, MEMS appears to be well-suited
as a real time clock (RTC) since they have very low power and size requirements, are
reliable at low frequencies, and noise/jitter is not as much of a concern with an
RTC. (See Application Specific Clocks for more information on RTCs.) Any oscillator
and circuitry on an integrated single chip, etched in the same silicon or similar
substrate, has all of the components on a single die, giving more precise operation
and improved performance over temperature.