What Are Piezo-Phototronics? Liam Critchley
Piezo-phototronic materials share many characteristics with piezotronic materials that help modulate charge carriers and electric currents at different semiconducting interfaces, but they also have photoexcitation properties that enable them to enhance a range of optoelectronic devices.

The Potential for Nanomaterial Inks in Electronic Devices Liam Critchley
Electronic devices are advancing in many ways, and are moving towards very small devices and components, as well as new types of flexible technologies. The potential for nanomaterial inks to be used as a flexible and conductive circuit is huge for flexible, wearable and printable electronic devices.

Why Nanowires Could Be a Big Thing for Electronics Liam Critchley
Nanowires are 1D nanomaterials with efficient electron transport properties where the electrons flow along the long axis of the wire. The electronic conductivity properties, which are realized through quantum effects, could be useful for a range of innovative electronics.

An Introduction to Nanoelectronics Liam Critchley
As components need to get smaller to accommodate consumer needs, manufacturers need a way of doing this. Nanoelectronics is the creation of electrical components using nanomaterials that can not only reduce the size of the device, but also provide the same, if not better, performance.

Harnessing Energy with Nanogenerators Liam Critchley
Different nanogenerators can generate enough electricity to power a small device through kinetic movements within the device, or by harvesting thermal energy. Even though the amount of electricity generated is small, it is enough for many small remote monitoring devices.

All Authors

Show More Show More
View Blogs by Date