Improving Extreme Temp Performance in EV Batteries Adam Kimmel
Extreme temperatures can reduce EV range by up to 35 percent and negatively impact battery durability. Energy harvesting is emerging as a tool to trim these efficiency losses to optimize battery performance and increase charging speed.

How to Maximize the Efficiency of Energy Harvesting in Electronics Adam Kimmel
Energy harvesting requires a distinction between maximum power and maximum efficiency. Improved conversion efficiency increases power for the same input energy; however, this does not necessarily mean the highest power. Here is how you can maximize the efficiency of MCU energy harvesters.

New Tech Tuesdays: These 3 EMI-Sensitive Solutions Can Manage the Static Tommy Cummings
The automotive electrical environment has a lot going on, with several applications being electromagnetic interference (EMI) sensitive. This means deploying switching regulators that limit the noise and don't exacerbate EMI concerns for design engineers.

Optimizing Power Designs with OptiMOSâ„¢ 6 MOSFETs Paul Golata
You have the power to optimize your power designs. Infineon Technologies’ OptiMOS™ 6 Power MOSFET 40V family offers class-leading cutting-edge power MOSFETs for the highest power density and energy-efficient solutions.

Build Smaller, Higher Efficiency DC-DC Converter Designs Paul Golata
Murata’s unique architecture for buck regulators has demonstrated an almost two-times reduction in footprint and a one-third reduction in height with significant improvements in power efficiency, transient performance, and electromagnetic interference (EMI).

Infineon MERUSâ„¢ Audio Amplifier Music to Our Ears Paul Golata
Skip the design and get to your development quicker so you can listen to music. See how Infineon MERUSâ„¢ Audio Amplifier HAT ZW for Raspberry Pi single-board computers (SBCs) enables the rapid development of wireless music streaming, along with low-power usage and efficiency.

Moving from Smart to Brilliant Energy Jon Gabay
Making energy use more efficient on a device is common. Doing it with a distributed random needs-based environment is more difficult. Appliances that can work together to assure peak-demand load conformity will have an advantage over those that don’t.

Going Off-Grid Efficiently With MicroGrids Paul Lee
Microgrids are becoming popular for environmental and dollar cost savings. However, adoption is dependent on efficient power conversion electronics enabled by the increasing use of wide bandgap semiconductors.

All Authors

Show More Show More
View Blogs by Date