Bench Talk | Page 105
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
DAS and the Wild West Barry Manz
If you’ve been following the progress of Distributed Antenna Systems (DAS) and small cells and find yourself with more questions than answers you’re not alone. Many very knowledgeable people I speak with on this topic find it difficult to define with any certainty precisely what is going on in this environment.

Wonder Twins Powers Activate! Lynnette Reese
Open source is part of some totally cool ideas. The NFC ring by Jon MecLear, funded by crowdsourcing, is one example of how technology migrates into every area of our lives. NFC stands for Near Field Communication. This ring looks like a wedding band. But think about how easy it would be to wear a ring that could replace the fob to unlock your car, automatically unlock your smart phone or tablet when you pick it up, and unlock your front door.

Doing the Low-Power Limbo John Donovan
Back when they still made vinyl records the Limbo was a popular dance craze. Imported from the Caribbean via Chubby Checker, you’d try to dance yourself under a horizontal bar without falling flat on your back. The lower the bar went the more people would clap—up until the point where you crashed out and everyone laughed. The challenge was, “How low can you go?”

Navigating Kids and Technology as a Dad Justin Risedorf
Technology connects me to work, news, and entertainment 24/7. That type of access has its benefits, but when left unchecked, it can dominate my time, distracting me from the things that matter most. New research on the patterns of technology used by parents has me wondering, what are my kids learning about life as they watch me check my phone for the nth time tonight?

Bowling, Baseball and Battles: What they have in Common with LEDs Paul Golata
I’m a guy. That means I’m extremely competitive. When I was dating my wife, Dianna, and if we played any games together, I would be relentless in my competitive approach and make sure I crushed her, demonstrating my total domination of all things. Then she asked me to bowl. That stupid ball never seems to roll where I aim! Dianna was a good bowler and took pride in silently racking up the pins, while I stewed in my anguish. In bowling the perfect score is 300. I can hardly get to half of that. In baseball the mark of an excellent hitter is to have a career batting average of .300 or better. As of 2013 there have been 205 players who have batted at least .300 (minimum of 3,000 plate appearances). This is a small number when you think about the number of players who have ever played the game.

5G: Coming Sooner than Later Barry Manz
Now that most of us have smartphones with LTE capability, life is good. Video streams nicely, downloads are quick, and if you happen to be standing next to a base station data rates can be truly impressive. It won’t be long before LTE Advanced shoves LTE aside with data rates 10 times faster, which means we will be able to download HD movies very quickly and do virtually anything else almost instantly. That however, is apparently not enough for the wireless industry, if developments in South Korea and the European Union are any indication.

Don’t Burn Out! Calculating LED Current Limiting Resistor Mike Parks
Light Emitting Diodes (LEDs) are one of the most fundamental output devices used in open source projects. They provide you a simple way to provide feedback to a user on the status of what’s going on in a circuit. A popular use is a power indicator to let the user know if a device is on. But connecting an LED directly to a power source can cause an LED to burn out. You have to utilize a current limiting resistor in series with the LED for protection.

LED Technology and Art - A Greek Geek Perspective Paul Golata
I can’t draw! I can’t paint! I can’t make anything with clay besides a sorry looking snake and I made one sorry looking ash tray in my elementary school days. I have always wanted the gift of being able to produce art. I am in no way an artist! I saw this picture on the internet as one of the “photos” of the day and it grabbed my attention. This artist is using LED technology in his art in an interesting way.

The “Death of the Downconverter”? Not Just Yet Barry Manz
The impact of converting analog signals to digital form is one of the greatest advances the electronics industry has ever achieved. Although today almost every consumer, industrial, commercial, and military system depends on this capability, one of the last remaining outliers is directly converting analog signals at microwave frequencies into digital data streams without using large amounts of intervening microwave hardware (i.e., downconverters).

Fool Me Once: April Fools' Gags 2014 Erik Smith
Another April Fools' Day is upon us, and with it comes a fresh helping of tech-based pranks. Followed by an inbox full of amazed e-mails from gullible family and friends. Here's a helping of some of my favorite high-tech hijinks from around the web, in no particular order:

All Authors

Show More Show More
View Blogs by Date