The Vincotech A1035-H GPS antenna module provides what designers of GPS applications need most: high performance and new features at a low system cost. The Vincotech A1035-H GPS antenna module is built around the SiRF GSC3 chip set and shows an excellent sensitivity of -159dBm along with a power consumption as low as 86mW. This Vincotech GPS module not only has an on-module antenna, but it also supports an active external antenna. Designers can choose between the two antennas simply by changing the state of an input pin. The A1035-H is a surface-mount device that assures low assembly costs and requires no manual operation.