|    Change Country Change Location USD
United States United States

Please confirm your currency selection:

US Dollars
Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

Get to the Root of Motor Control with the Freescale Kinetis KV1x MCUs Available from Mouser

July 2, 2014 - Mouser Electronics, Inc. is now stocking the Kinetis© KV1x Microcontroller Family from Freescale Semiconductor. The Kinetis V Series V1x MCU family is the entry point to Freescale's new Kinetis V series, a scalable microcontroller (MCU) family that targets digital motor control applications. Based on a 75MHz ARM® Cortex‑M0+ core, the Kinetis KV1x family includes an integer divide and square root co‑processor that reduces the CPU load caused by demanding motor control algorithms.

The new Freescale® Kinetis KV1x Microcontroller Family, available from Mouser Electronics, boasts significant improvements in performance compared to other microcontrollers in its class. These improvements allow cost‑sensitive applications to take advantage of the enhanced efficiency and precise speed/position control offered by the latest motor control devices. The KV1x microcontrollers include an advanced analog and timing peripheral set with two 12/16‑bit analog‑to‑digital converters (ADCs) capable of 1.2Msps in 12-bit mode for fast signal acquisition and conversion, a 12-bit digital‑to‑analog converter (DAC), and two analog comparators that reduce bill of material (BOM) costs while providing fault protection against over current/voltage conditions. Multiple independent Freescale FlexTimers generate high resolution PWM signals, while a programmable delay block accurately detects rotor positions in sensorless applications.

In order to help meet compliance with IEC‑60730 safety standards for household appliances, Kinetis KV1x MCUs have two independent watchdogs to help ensure the safe operation of on-chip firmware. In addition, a hardware Cyclic Redundancy Check (CRC) engine allows safety verification of the validity of the contents of the Flash memory, as well as checking the integrity of all onboard serial communications.

Target applications for Kinetis KV1x series MCUs include brushless DC motor control, stepper motor control, and low voltage DC motor control.

To learn more, visit:
http://www.mouser.com/new/Freescale-Semiconductor/freescale-kinetis-v-mcu/ .

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Media Communications Manager
(817) 804-7764