Mansfield, Texas, USA — December 27, 2010 - Mouser Electronics, Inc., known for its rapid introduction of the newest products, today announced it is stocking new product from Exar.
Exar SP337E multiprotocol transceivers contain both RS-232 and
RS-485/422 line drivers and receivers. The RS-232 mode provides three
drivers and five receivers to support all eight signals commonly used in
the DB9 serial port connector (3TX/5RX). In RS-485 mode the device
features two independent high speed RS-485/422 transmit and receive
channels (2TX/2RX). The Exar SP337EB multiprotocol transceiver
features a maximum data rate of 250kbps in RS-232 mode and a maximum
data rate of 15Mbps in RS-485/422. The Exar SP337EU features a
maximum data rate of 1Mbps in RS-232 mode and a maximum data rate of
15Mbps in RS-485/422 mode. SP337E multiprotocol transceivers
require only four 0.1µF capacitors for complete functionality. To learn more, visit http://www.mouser.com/exarsp337e.
With its broad product line and unsurpassed customer service, Mouser offers customers the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches over 6.7 million products to locate over 1.8 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, Inc. is an electronic component distributor, focused on the rapid introduction of the newest products and technologies to electronic design engineers. Mouser.com features more than a million products online from more than 400 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 280,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility in Mansfield, Texas.
For more information, visit www.mouser.com.
About Exar
Exar Corporation powers connectivity with an extensive array of power management, communications, and interface silicon solutions. Exar's power management ICs are used in a variety of applications and include LDOs, DC/DC switching regulators, PWM controllers, charge pumps, and microprocessor supervisors. The products are designed for use together to a create complete power management systems but can also be used as standalone solutions. Exar also offers online design tools to help designers create customized solutions using Exar products. For more information, visit http://www.exar.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.