© 2005 Mouser Electronics, Inc. is a registered trademark of Mouser Electronics Inc. All other trademarks and service marks are the property of their respective owners.

 
 

Mouser Electronics
Go to Mouser.comView the NEW Suppliers on Mouser.comView the NEW Products on Mouser.comView the NEW Technologies on Mouser.comView or Download Mouser's Latest CatalogOrder Electronic Components from Mouser.com

 
 

Microchip ZigBee Demonstration Kit
Mouser Receives 10 Awards
KEMET MLCC Capacitors
Mouser Special Edition CD Catalog
Phoenix Contact Industrial Ethernet
Mouser Environmental Commitment

See More New Products at Mouser.com

  ?   The #1 supplier of 8-bit microcontrollers announces its new ZigBeeTM Technology Demonstration Kit. The PICDEMTM Z demonstration board is an easy-to-use ZigBee Technology wireless communication protocol development and demonstration platform. The kit includes the ZigBee protocol stack and two PICDEM Z boards, each with an RF daughter card.

Click here for more information on Microchip’s HOT products.

 
  Mouser receives 10 Awards from Nine of its suppliers at the recently held Electronic Distribution Show & Conference (EDS) in Las Vegas! Suppliers cited several reasons for the numerous honors, including double-digit sales growth, FAST New Product roll out, and Mouser´s commitment to teamwork. All in all, Mouser is easy to do business with!

Click here for more information

  ?  
  ?   Why not buy your High Capacitance MLCC capacitors from the industry leader in customer service, quality, delivery, reliability, and RoHS compliance?
KEMET is dedicated to meeting and exceeding the industry´s ever-increasing high capacitance needs through continuous enhancement and expansion of our High Capacitance MLCC portfolio with the latest extended capacitance value offerings in X5R and X7R dielectrics, ranging from 1 to 47 µF in the 0402, 0603, 0805, 1206, and 1210 case sizes at voltage ratings of 6.3V, 10V, and 16V.

Click here for more information on KEMET´s HOT new products

 
  Mouser Electronics introduces its NEW Special Edition CD featuring our latest 1,532-page print catalog, along with 131 supplier catalogs featuring Semiconductor, Optoelectronics, and Embedded Solutions products.

This CD is the first of three special edition CDs to be produced. The second version will contain Mouser´s catalog with supplier catalogs featuring Passive Components and Circuit Protection products. The third CD will contain Mouser's catalog featuring supplier catalogs for Interconnect, Electromechanical, and Power products.

Click here for more information


  ?  
  ?   Industrial Strength Ethernet Devices from Phoenix Contact are quick, rugged and reliable connections on the factory floor. Ideal for main control cabinet applications, installation time is reduced with our pluggable Ethernet connections and fingertip locking latch that provides a simple, fast, and secure connection. These devices are rated IP67 (splash-proof, dust-proof, and corrosion-resistant), with male and female inserts shielded to tolerate EMI.

Click here for more information on Phoenix Contact products

 
  Visit www.mouser.com/environmental to get the latest information on the various RoHS, WEEE, Packaging and Waste, Battery initiatives and directives from the European Union and around the globe. Mouser Electronics and our parent company, TTI, Inc., are committed to an environmental-friendly leadership position in the industry. Check out our suppliers’ RoHS statements, glossary of terms, and useful resources to further understand the challenges and opportunities brought about by these environmental initiatives.

Click here for more information

?

 
 
 
We respect your privacy. Click here to read our privacy policy.

If you’d like to contact us, please don’t reply to this e-mail. Visit our Comments page instead.

If you would prefer not to receive Mouser New Technology emails, please click here to send us an e-mail or write to Mouser Electronics, Opt Out, 1000 N. Main Street, Mansfield, TX 76063.