|    Change Country Change Location USD
 
United States United States

Please confirm your currency selection:

US Dollars

Mouser is pleased to sponsor the foremost event of the year covering new advancements in motion control and power electronic technology. It’s one conference you don’t want to miss.






Conference Program


  • Wednesday, January 29
  • Thursday, January 30

7:00 AM - Registration & Continental Breakfast
8:00 AM - Opening Address
8:05 AM - Keynote Presentation

Industrial Motors and Drives – A Global and North American Market Update
Hear IHS's latest analysis of the global industrial motor and drive markets. The presentation will summarize how these markets are segmented by product type, geographic region and industry sector. In addition to presenting market data, the presentation will describe the current competitive environment for these products, including an analysis of the leading suppliers to these markets.
Mark Meza, Principal Analyst, Motion & Mechanical Power Transmission, IHS

9:15 AM - Featured Presentation

What's New in Motor Technologiese
There are two major motor technology driving forces in two different segments of motion control. The first involves power efficiency and the second is torque density. Power efficiency improvements are driven by the DOE. A recent development using sheet metal stators and multiple dimension Halbach magnet arrays has significantly increased the power efficiency levels in motors below 50 horsepower (34.3 Kw) used in various speed applications.
Dan Jones, President, Incremotion Associates, Inc.

10:00 AM - Exhibit Hall Opens / Networking Break

10:30 AM

Efficient Operation of Stepping Motors
Stepping motors are highly popular because they offer high torque at low speed, and high precision at low cost. These unique benefits enable the design of direct drive systems, eliminating the additional cost and complexity of gearboxes. However, stepping motors are not known for being energy efficient and, because if overloaded they tend to stall and lose step awareness, they are usually over-designed for the application with a safety margin of at least 50 percent. This presentation will discuss two new techniques that overcome these challenges.
Michael Randt, Founder and CEO, TRINAMIC Motion Control
Dr. Stephan Kubisch, Head of R&D, TRINAMIC Motion Control

Active Disturbance Rejection Control: A Replacement For PID
Active Disturbance Rejection Control (ADRC) is a technology that proactively estimates and automatically compensates for system disturbances with just a single adjustment. With motion control expertise embedded on chip, ADRC can replace PID control and expedite motor control tuning and development. Discover how having embedded motion control expertise on a chip can reduce energy and cost while simplifying design and improving performance in a variety of motor and drive applications.
Sharon Fay, Director of Product Management, LineStream Technologies

11:10 AM

New DC Motor Design Improving Power Density and Noise Level
A new motor design has been developed to meet the demanding challenges that comes when designing in micro drives into a given application. The motor’s improved efficiency, higher power density, patented ironless rotor and quiet operation insures a highly dynamic drive solution. This presentation provides an overview of the technical innovations in this new technology of DC drives, explains the most recent innovations, the unique assembly process and how they benefit manufacturers and their customers with the advantage of customized configurations to meet individual specification.
Matt Badger, e-Business Agent, maxon precision motors

Illustrations for a Dynamic Braking Chopper Solution in A Medium Voltage AFD
As an induction machine’s rotor is accelerated to a desired process speed the electromagnetic torque is positive. Therefore, real power is supplied to the machine and it operates in the ‘motoring’ mode. However, when the rotor is slowed, yet still positive in speed, the difference in load and inertia can result in negative electromagnetic torque. This ‘generating’ mode machine power can be absorbed in adjustable frequency drives using a dynamic braking chopper. Learn how the chopper is sized for a full speed ramp stop.
Stan Simms, Senior Product Design Engineer, Eaton Corp.

11:45 AM - Networking Luncheon


1:00 PM

A Look at Soft Magnetic Composites for Motor Design
The benefits of soft magnetic composites (SMCs) have been promoted for several years but the have been slow to enter many application areas. Recent advances in SMC technology may change this and open many opportunities for designers to improve the power density and efficiency of motor designs through the use of SMC instead of conventional motor laminations. This presentation will share some observations using specific examples where the performance of SMCs can be directly compared to the performance of conventional laminated motor designs.
George Holling, Technical Director, Rocky Mountain Technologies, Inc.

Industrial Ethernet Comparison for Motion Control Applications
Several communications Ethernet based busses have been developed so far to handle real-time control for motion and distributed I/O. Which of these standards is best for your application requirements, considering axis count, cycle time, jitter, EMC robustness and network topology. Further aspects to be covered in this talk include: hot-plugabilty, safe motion and implementation and licensing costs.
Sari Germanos, Technology Marketing Manager, B&R Industrial Automation Corp.

1:40 PM

High-Speed Permanent Magnet Synchronous Motor Close Loop Control and Drive System Design
High speed motors can achieve high power density compared to conventional designed machines. This makes them suitable for a broad range of applications. With high speed, close loop control and drive system design become challenging. In this presentation, we report the close loop control and drive system design of a 2-pole 24-slots super high speed PMSM. The rated speed of the motor is 150 krpm and the rated output power is 3 kilowatts. The testing process is also going to be discussed.
Yang Hu, Center for Advanced Electric Machinery (CAEM), University of Central Florida

Sensorless Control Methods for Brushless DC, PM Synchronous and Induction Motors
Discover various sensorless control methods practically used in industry and compare technologies for dynamic performance, robustness, limitations, complexity of implementation and tuning issues. Topics include traditional back emf detection method, carrier injection method, direct field orientation, extended Kalman filtering, Luenberger observers, and sliding mode observers. Several different starting methods are presented as well.
Dr. Dal Y. Ohm, President, Drivetech, Inc.

2:20 PM

Emerging Electrical Motor Technologies
As the automotive, aerospace and industrial industries continue to evolve toward more energy efficient systems, new technologies are emerging. These new technologies are placing larger demands on motor materials in order to help improve motor efficiencies. Advances in Samarium Cobalt (SmCo) magnet technologies now allow for increased power densities at higher temperatures while carbon fiber sleeving technologies allow for increased operational RPMs.
Aaron Williams, Project/Magnetics Engineer, Arnold Magnetic Technologies

Innovations and Improvements in Single-Phase AC Motor Controls
Single Phase AC motors continue to dominate the low-cost, low-power air-movement markets and the change to increased energy efficient EC motors and more complex three-phase AC motors has been slow to happen. Innovations in using digital control techniques to improve speed control linearity and auto-adjust techniques will be covered in this innovative field. Improved performance combined with improved efficiencies will allow low-cost AC motors to meet new challenges of performance and energy savings.
Howard Abramowitz, President, AirCare Automation, Inc.

2:50 PM - Networking Break


3:15 PM

New Variable Flux PM Motor and Generator Design
Permanent Magnet machines have been attractive choice for many high power motor and generator applications such as Navy propulsion and other high power industrial applications. The new patented design of Variable Flux PM Motor/Generator offers possibility to utilize PM technology for high power applications without the typically associated risk factors and simplifies their control. Presentation will discuss several possible embodiments of the new design along with FEA and test results of a scaled down prototype machine.
Dr. Kolomeitsev, Advanced Motors Electromagnetics
Louie Finkle, Electric Louie, Inc.

Improving Reliability of Inverter Driven Motors with Shaft Voltage Testing and Bearing Protection
The bearings in AC motors operating on variable frequency drives (VFD) are vulnerable to shaft voltages that may be of sufficient amplitude to cause electrical discharges in the motors bearings. These discharges produce an electrical discharge machining (EDM) effect in the motor’s bearings that cause pitting and fluting and premature bearing failure. The shaft voltages may be detected and measured using an oscilloscope and a shaft voltage probe that touches the motor’s shaft while it is running.
Adam Willwerth, Product Manager, Electro Static Technology

3:55 PM

Novel Radial Amorphous Iron Motor
Amorphous iron is the most efficient magnetic material available for motors, especially at design frequencies exceeding 400 Hz. Five demonstration motors have been built; two of these motors are in test with more than 10,000 hours. The motor’s advantages over conventional approaches is to create higher efficiency motors wasting less energy, air cooled designs where competing motors are liquid cooled, and due to the lower heat loss, compact designs result in overall less material usage.
Andrew Hirzel, Radam Motors

The Advantages of (Really) Low Voltage Drive Systems
OEM’s have presented a growing number of new applications for brush and brushless DC motors using less than 50 volt source power. Depending on the application or industry, these OEM’s have compelling reasons for staying below this voltage threshold. This presentation will explain current market and regulatory conditions influencing OEM designers to stay below 50V source power. These conditions vary by industry segment; however they find synergy in the drive / motor solution.
Mark Lewis, Vice President – Marketing & Sales, Dart Controls, Inc.

4:30 PM

An Open Source Motion API
The advent of Machine to Machine (M2M) networking presents both an opportunity and challenge to the Motor and Drive industry, particularly for older applications that have yet to move to electronic control and higher efficiency motors. To get on the ‘Cloud” these cost sensitive applications need to balance accessing the application’s information and functionality, retaining tight control of critical real-time machine processes, and avoiding excessive added cost.
Gary Box, Chief Technical Officer, Software Defined Power

5:00 PM - Cocktail Reception



8:00 AM - Registration / Exhibit Hall Opens / Continental Breakfast
8:30 AM - Keynote Presentation

The Future Trends, Technology and Opportunities in Motor and Drive Systems
Join this panel of industry experts as they discuss new developments, including standards, technology updates new opportunities in motor and drive systems. Hear application specific challenges to improve performance and efficiency. Discover the expectations from the manufacturer to the OEM.
Alex Chausovsky, Manager & Principal Analyst, IHS
Dr. Kolomeitsev, Advanced Motors Electromagnetics
Thomas Wu, Professor, University of Central Florida

9:40 AM

Enhancements in the Electric Machine Cooling Analysis
New efficiency regulations for electrical machines are placing greater demands on electrical machine designers. Now, alongside an optimized electromagnetic design, the thermal analysis has also become increasingly important in the design process. In the same way that SPEED’s analytical approach supports the electric and electro-magnetic design, Motor-CAD’s speed and accuracy is invaluable to the thermal design. This presentation will describe the workflow from the initial machine design using SPEED to the thermal modeling with Motor-CAD.
Dr. Dave Staton, CEO, Motor Ltd.
Dr. Markus Anders, Electrical Machine Sector Manager , CD-adapco

High Resolution Hall Effect Encoders Provide High Accuracy Signals in Harsh Environments
There has been a migration from optical to magnetic motor feedback in recent years attributable to the advantages of modern integrated magnetic sensors which include cost, packaging and reliability in industrial environments. This presentation reviews the two most misunderstood performance characteristics of modern high resolution Hall effect encoders: how modern magnetic encoders deliver accurate signals in the presence of external magnetic fields, and how modern magnetic encoders deliver accurate signals with changes in air gap / relative position between the sensor and target wheel.
Mark Lacroix, Senior Development Specialist, The Timken Company
A. John Santos, Chief Engineer – Sensors, The Timken Company

10:15 AM - Networking Break

10:30 AM

Comparison of Power Quality Effects on Different Motor Technologies
Adverse power quality conditions detrimentally affect the performance of connected equipment, including electric motors. In the case of electric motors, some of the well-known effects include overheating, reduced efficiency, insulation damage, motor burn-out and motor tripping. Hear an overview and comparison of the effect of supply voltage abnormalities on different motor technologies such as induction motors, permanent magnet motors and motors connected to variable frequency drives.
Emmanuel Agamloh, Motors and Drives Consultant, Advanced Energy Corp.

11:10 AM

Practical Methods for Reducing the Losses And Harmonics Distortion in Industrial Motor Drive Systems
Discover a practical way of reducing the losses and harmonic distortion produced by the inverters and converters for industrial motor drive and motor applications. This is achieved by calculating or determining the effective minimum deadtime for the power switches in the drive. Application of these methods result in an industrial drive system that is smaller, more efficient and more reliable.
Dong Le, Director of Technology, Calnetix Technologies LLC

Boost Performance in Motion and Position Sensing Applications with Single-Chip Encoders
When designing systems with motion and/or position sensor feedback, advances in Single-chip encoder semiconductor devices offer designers higher integration, flexibility, performance increases, advanced configuration features, and cost reductions. By utilizing Single-chip encoders with built-in smart sensor technology, a highly flexible and configurable design can be realized for enhancing overall system performance.
Bruce M. Pride, Principal Engineer, iC-Haus AmericaC

11:45 AM - Networking Luncheon


12:45 PM

Bright Future for Electric Motor Efficiency Improvements
Motor system efficiency has improved significantly in recent years, yet there are still many additional gains that can be expected in the future. Both motor and drive efficiency improvements will be reviewed, and the three major motor technologies (induction, permanent magnet (PM) and reluctance motors) will all be examined. A special emphasis will be placed on covering emerging magnet materials that could improve PM motors. The drive improvement section will cover drive design and new drive components, as well as looking at novel ways to employ drives to improve system efficiency.
John Petro, Motor Design Consultant

1:25 PM

Drive to a Greener Future
Learn how to realize cost savings with state-of-the-art variable frequency drives technology. In many applications, variable frequency drives have the potential to return energy back to the facility power grid through regenerative infeed technology. Returns on Investment can be realized in as little as 3-6 months depending on the existing installation. Additionally, the concepts of energy efficiency and the financial incentives available for energy efficient installations will be reviewed.
Ken Kerns, Drive Technologies, Motion Control & Low Voltage Drives Marketing, Siemens Industry, Inc.

2:00 PM - Conference Conclusion


See more at: http://www.e-driveonline.com/conferences/conference-program/#sthash.vGmR3quU.dpuf