United States United States
Please confirm your currency selection:


ECIA Authorized Maestro Wireless Solutions Distributor

Maestro Wireless Solutions

Maestro Wireless Solutions, established in 1980, simplifies communication between machines by designing and delivering an extensive portfolio of state-of-the-art wireless products and services adapted to the needs of the demanding Machine to Machine (M2M) market. With a focus on modems and Gateways, including products like GPS and embedded modules, Maestro Wireless Solutions offers 20 different modems especially developed for targeted vertical applications. Maestro Wireless Solutions has become a market reference in terms of robustness and cost effectiveness with large scale development in harsh environments such as Russia, India, and Southern Africa.

Maestro Wireless SiRFstar IV GPS Receiver Modules & Eval Kits

Maestro Wireless SiRFstar IV GPS Receiver Modules offer some of the most critical features in the GPS market--high integration, high performance, and a reduced time to market. In the A2035-H module, the combination of a fully enhanced, Flash-based SiRFStar IV GPS engine and a high directional patch antenna eases the process of integration in tough electrical environments. The A2200-A offers ROM-based SiRFStar IV and a smaller form factor, and requires a trace for the appropriate antenna. Maestro Wireless SiRFstar IV GPS Receiver Modules provide extreme low power operation and ultra fast TTFF, and their highest sensitivity allows for use in the most demanding conditions. Also available, the Maestro Wireless SiRFstar IV GPS Evaluation Kits allow easy evaluation of the SiRFstar IV GPS Receiver Modules. The eval kits offer quick access to the serial ports and the most important I/O lines of the modules.

Maestro Wireless Solutions Heritage GPRS/EDGE Main Unit

Maestro Wireless Solutions Heritage GPRS/EDGE Main Unit combines industrial-grade design GSM/GPRS/EDGE technologies with pluggable boards for Machine-to-Machine applications. This modular and scalable design concept transforms the Heritage into a Multitechnology Gateway which features a powerful operating system offering Download Over The Air capabilities and innovative embedded applications. Being customizable both in terms of hardware and software, the Maestro Wireless Solutions Heritage GPRS/EDGE Main Unit is the best tailored solution of choice in direct response to market needs.

Maestro Wireless Solutions A1035-H GPS Antenna Modules

Maestro Wireless Solutions A1035-H GPS Antenna Modules provide what designers of GPS applications need most: high performance and new features at a low system cost. The Maestro Wireless Solutions A1035-H GPS Antenna Modules are built around the low power SiRFStar III GSC3 chip and show an excellent sensitivity of -159dBm along with a power consumption as low as 86mW. These Maestro GPS Modules not only have an on-module antenna, but they also support an active external antenna. Designers can choose between the two antennas simply by changing the state of an input pin. The A1035-H is a surface-mount device that assures low assembly costs and requires no manual operation.

Maestro Wireless Solutions A2100 SiRFstarIV GPS Modules

Maestro Wireless Solutions A2100 SiRFstarIV GPS Modules answer designers' GPS challenges by enabling the fastest acquisition and tracking with the latest SiRFstarIV technology. The Maestro Wireless Solutions A2100 SiRFstarIV GPS Modules are an appropriate solution for all telematics and power-sensitive mobile consumer application devices, fully answering the demand for lowest power consumption with SiRFaware™ technology. The removal of jammers both facilitates designs of new products and guarantees operation even in hostile environments. These Maestro GPS Modules use SiRFaware™ technology for constant Hot Start, and feature the best acquisition sensitivity--during acquisition or while tracking--making them ideal for operation in many different environments and under the toughest conditions.