New Functions & Benefits
- An internal, latched locking mechanism on the hood
- Multiplies the potentials in the connector with Han- Yellock ® modules
- Use of Han- Yellock ® modules with adapter frames
- Insulators can snap into the front or back walls of the housing
- Protected Earth contact (PE) in crimp or Quick Lock termination
- Less article number and less inventory when purchasing
- Less wiring work within a machine when planning for the electrical and mechanical layout
- Less steps in the work flow and quicker assembly
- Reduced down times because of the latched locking mechanism and maintenance-friendly design
|
Han-Yellock® Connector System
New design of Han® Connector extends functionality
HARTING introduces the Han-Yellock® Connector System, a new product series which retains the core functionality of the respected Han ® connector line and offers significant differences in size and shape to improve functionality in the form of variability, multiplied potential, simplified handling, reduced incidence of errors, and maximized safety. The new approach of this series makes many new functions possible.
Design Overview
The HARTING Han- Yellock ® Connector System interface consists of a housing, bulkhead mounting on the housing side and a carrier hood with cover on the cable side. The system can be used with a variety of insulators and contact inserts in order to establish an interface. The Han-Yellock® offers the following features when assembling components:
- Han-Yellock ® modules require only male crimp contacts
- The PE is contacted on the housing; it can be connected with crimp and/or Quick Lock contacts
- The Han-Yellock ® hoods/housing are not plug-compatible with all other Han® hood/housing series.
Locking Feature HARTING's Han-Yellock® features a patented internal locking mechanism that makes connections and disconnections safe, simple, and quick - even under harsh industrial conditions. The locking takes place as the cable and device sides are simply joined together and stainless steel springs snap into place. A red ring around the perimeter of the push button will be visible if the housing halves do not snap together properly. An integrated press-button blocking feature can be rotated 90º to prevent accidental opening of the connector.
Modules This Han-Yellock ® series enables an improved approach and strategy for electrical planning and procurement. For assembling the Han-Yellock® connector, only male crimp contacts are needed. The conduct between the two male contacts is made by multipliers. This concept allows a 1:1 wire to wire arrangement and the use of bridges. Two to five contacts can be arranged. It does not matter if the bridge attachment is inserted on the cable side or the housing side of the connector. In the past, terminals blocks have been responsible for the function of multiplying potentials. Now, this function has been integrated into the connector for a quick, compact and easy-to-service solution.
Adapter Frame Han-Yellock ® series interfaces can be established using the adapter frame. The connection is based on a male/female contact arrangement.

|