DLP High Speed USB Microcontroller ModuleDLP High Speed USB Microcontroller Module combines an FTDI FT2232H USB to UART IC interface with a Texas Instruments microcontroller to form a rapid development tool. The DLP High Speed USB Microcontroller Module provides a cost-effective, microcontroller-based method of interfacing an electronic peripheral to a host computer via USB. The MSP430F2618 microcontroller is preprogrammed with basic functionality for accessing the port pins and can be reprogrammed with user firmware via a 10-pin header using a device programmer (sold separately). No in-depth knowledge of USB technology is required as all USB protocols are handled automatically by the on-board FT2232H and its support circuitry. The MSP430F2618 microcontroller is USB 2.0 Hi Speed compatible. The DLP-2232MSPF also combines the same USB interface used in the DLP-2232H module with a Texas Instruments microcontroller with internal FRAM to form a rapid development tool. The MSP430FR5739 microcontroller can be reprogrammed with user firmware via a 12-pin header using the MSP-FET430UIF device programmer/debugger (sold separately).
|