The new Mouser Enhanced Catalog is the next generation of convenience in catalog shopping. The online catalog is available from the "dog ear" in the right corner of the Mouser homepage. After a quick download of Microsoft's Silverlight, you can search for products by partial keywords, part number (Mouser or supplier), supplier name, or product categories. You can easily add parts to your online cart without ever leaving the catalog. The catalog remembers the last 20 catalog page views and allows you to bookmark up to 100 pages. Nothing could be easier!
| Catalog Headers The Control Panel appears at the top of the Catalog Viewer Application.
 |
|  |
|
|
|  | Allows you to bookmark up to 100 pages into the Bookmark tab in the Control Panel.
|
| Prints the catalog page in PDF.
|
| Goes to the catalog Help Center on Mouser.com.
|
| Links to your shopping cart on Mouser.com.
|
|
| Control Panel The Control Panel appears in the left frame of the Catalog Viewer application.
| 
| The Search Catalog tab contains a text field to enter key words and/or Mouser or supplier part numbers. The green search button will return all results from the entire catalog. Simply click on your selection to view the catalog page in the Catalog Viewer to the right.
The Browse Products tab displays product categories. Continuing drilling down until you see the catalog page you want.Simply click on your selection to view the catalog page in the Catalog Viewer to the right.
The Browse Suppliers tab displays all suppliers and allows the user to drill down to the catalog page desired.Simply click on your selection to view the catalog page in the Catalog Viewer to the right.
The History tab lists the last 20 catalog pages viewed by the user. The pages can be viewed again by selecting the desired page. When the 20 page limit is reached, the oldest catalog page in the list is automatically deleted.
The Bookmarks tab lists up to 100 catalog pages bookmarked by the user to quickly reference at a later time. Bookmarks are created by selecting the "Add Bookmark" button in the Header area. Bookmarks can be deleted by selecting the red "X" that appears to the left of each bookmark when the user rests over the bookmark.
|
| Catalog Page Viewer
The Catalog Page Viewer is located in the center of the page. The viewing area displays a catalog page that has been selected from the Control Panel area to the left. At the top of the area, the catalog page number is displayed, as well as scrolling arrows to the left and right to view adjacent catalog pages, and a Zoom button to determine the magnification desired. A sample page is shown below. 
The catalog page is displayed in the large center area. Mouser part numbers are highlighted and linked to a pop-up with product details (image, specifications, and purchasing information) and a "Buy" button if you desire to add the part to your cart. If multiple part numbers are found, a message will appear to ask if you would like to close the catalog viewer and go directly to Mouser.com to search for the part. Closing the Product Detail pop-up will re-enable the Catalog Viewer. |
| Microsoft Silverlight
All that is required is a free, quick (less than 10 seconds) download of Microsoft's trusted Silverlight. Silverlight enables the sophisticated internet applications required to enjoy the complete Catalog experience. Silverlight is installed as a free browser plug-in approximately 4MB in size.
Minimal Requirements
| Components |
Requirement |
| Personal Computer running Windows |
X86 or x64 500-megahertz (MHz) or higher processor with 128-megabytes (MB) of RAM |
| Mac OS 10.4.8+ (PowerPC) |
PowerPC G4 800-MHz or higher processor with 128-MB of RAM |
| Mac OS 10.4.8+ (Intel-based) |
Intel Core Duo 1.83-gigahertz (GHz) or higher processor with 128-MB of RAM |

For more information about Microsoft Silverlight, visit: Microsoft Silverlight Home Page
|
|