Contact Mouser (USA)  (800) 346-6873     |     Feedback  
View Cart     |     Change Location  USD
United States United States

Please confirm your currency selection:

US Dollars
Home » Applications & Technologies » USB 3.0 SuperSpeed Technology
Applications & Technologies

Universal Serial Bus (USB) is the most successful peripheral interface in the history of the personal computer. USB is a standard connection interface between computers and digital devices. It enables the easy transfer of data through a direct connection or cable. USB was created with simplicity of use in mind, and thus “plug-and-play” became the expectation as drivers loaded themselves and printers, external hard drives, and other peripherals “just worked.”

Click on a category to learn more about USB 3.0.
Host Controller

The USB host controller, often simply referred to as “the USB host,” typically resides in a computer or head-end system. The host controller acts as an interface to move data between the computer and USB bus-resident devices by processing data structures, initiating transactions, and sending the data as packets over the USB bus. It can control several USB ports. Information flow towards the host is called “upstream” traffic and the flow of information away from the host is referred to as “downstream” traffic. The USB specification requires the host controller to include a “root hub,” which provides data flow control for the bus.

» View All Host Controllers for USB 3.0

Hub

Hubs are the supporting backbone of communication in the USB bus network. A hub in the host controller, called the root hub, provides data flow control at the highest protocol level of the USB network, which is physically nearest to the computer, or head end of the system.

» View All Hubs for USB 3.0

Transceiver (PHY)

A USB transceiver is a physical layer device that prepares data for transmission and then sends to, and receives data from, another transceiver. The transceiver detects connection and provides the low level USB protocol and signaling. The term “transceiver” indicates an implementation of both the transmit and receive functions. It transmits and receives, encodes and decodes data, provides error indication, implements buffers to stage data until it can be managed, and adjusts for the clock rate from the serial stream on the USB SuperSpeed bus to match that of the “link layer” higher up on the communication stack.

» View All Transceivers for USB 3.0

USB to SATA Bridge

This device is used to provide USB 3.0 connectivity to storage devices such as hard disk drives, optical drives and other SATA-dependent devices. It can be used to implement both storage and human interface device class devices for USB. It supports both generation 1 & 2 SATA speeds (1.5 Gbps & 3.0 Gbps, respectively) and includes a Cortex M3 microcontroller. Serial peripheral interface (SPI) and pulse width modulation output are included as well as provision for some general purpose I/O.

» View All USB/SATA Bridges for USB 3.0

Re-driver/Equalizer

USB 3.0 will be targeted initially at the PC market and in devices requiring high rates and volumes of data transfer, such as external storage, consumer electronics, and communications devices with increasing amounts of storage. High frequency signals are subject to problems with signal quality. Signal conditioners can help by filtering out anything above the expected ceiling frequency, and can “re-drive” the signal by retransmitting at increased signal power, effectively “re-driving” it through the signal path. USB is a consumer-friendly technology. Cable lengths for USB devices are not necessarily going to remain fixed at the length of the cable that came in the box. Therefore, the re-driver should continuously monitor the signal and dynamically equalize (or adaptively balance) itself in order to optimize the signal.

» View All Re-drivers/Equalizers for USB 3.0

Plugs/Receptacles

USB plugs and receptacles are meant to reduce human error by their unique shape; they fit together in only one way. USB plugs and receptacles come in Type A (typically connecting to hosts or hubs) or Type B (typically connecting to devices) and 3 sizes: standard, mini, and micro. Type A plugs always face upstream, Type B faces downstream.

All USB devices (or peripherals) have an upstream connection to the host and all hosts have a downstream connection to the device. USB 2.0 plugs will fit into USB 3.0 receptacles but do not contain the extra wires needed to convey SuperSpeed communications. Note that USB 3.0 Type B plugs do not fit into USB 2.0 receptacles. A USB 3.0 device going to a USB 2.0 host, for example, will only work with a USB 2.0 cable assembly.

» View All Plugs for USB 3.0

» View All Receptacles for USB 3.0

Cable Assemblies

There is no set standard on cables for USB, but rather for performance of the cable or system. USB 3.0 operates at data rates of up to 5 GHz by employing data-doubling techniques on a 2.5 GHz signal. Higher frequency signals suffer notably more signal losses than lower frequencies, so signal quality can be greatly affected with lower quality cables. To avoid signal degradation, higher-quality thicker-gauge cabling should be used with USB 3.0 devices.

» View All Cable Assemblies for USB 3.0

ESD

If you have ever been zapped by a socks-wearing kid who has just discovered static charge build up, you have experienced ESD first hand. ESD is like a miniature, localized lightning bolt caused by an electrical discharge. ESD can have seriously damaging effects on an integrated chip or system, or can cause poor performance or failure later on by merely weakening the circuits.

ESD protection should be used where ESD exposure can occur, and is recommended for data cables exposed via their connection points such as USB cable assemblies.

ESD can also be a periodic weak ESD that eventually breaks down the circuit. Devices may escape detection in the factory test harness, but are going to suffer a shorter product life. ESD may occur on any pin that is exposed to its environment. Common mode chokes can also be helpful in reducing, but not eliminating, ESD caused by transmission lines.

» View All ESD Protection for USB 3.0

Chokes

Common Mode Chokes are often placed at the base of a USB connector to reduce noise coming from the cable. Common mode choke coils consist of two or more magnetically combined coils that act to isolate unwanted AC frequency currents from a main circuit via two methods: common mode noise rejection and by creating a signal boundary at a defined cut-off frequency. Therefore, chokes can be seen as signal conditioners of a kind. Note that chokes are not full ESD (electrostatic discharge) protection devices, but can help reduce aspects of ESD system upset in addition to their main function of general noise reduction.

» View All Chokes for USB 3.0

Switches

USB 3.0 Switches provide smooth transitions. By maintaining low resistance and impedance, the signal switch can keep insertion losses down and preserve the signal so that no glitches are reflected back to the transmitter, thus helping to maintain a good quality signal.

» View All Power Switches for USB 3.0

» View All Signal Switches for USB 3.0

Clocks

USB 3.0 requires a Clock. Clock technology is more expensive and more complicated at higher frequencies. A lower frequency clock can be used and then multiplied to achieve the desired clock rate; however any jitter (error) is also multiplied. (Jitter is shakiness in the signal, caused by electro-magnetic radiation or the influence of nearby signals.) Circuitry supporting clock function should be selected for low noise.

» View All Clocks for USB 3.0

Featured Products
Cypress Semiconductor EZ-USB® FX3 SuperSpeed USB Controllers

EZ-USB® FX3 SuperSpeed USB Controller enables developers to add USB 3.0 functionality to any system. EZ-USB FX3 has a fully configurable, parallel, General Programmable Interface (GPIF II™) which can connect to any processor, ASIC, or FPGA. Integrating USB 3.0 and USB 2.0 physical layers with a 32-bit ARM926EJ-S processor, the FX3 provides exceptional processing power, great flexibility, and data transfers as high as 320 MBps from GPIF II™ to USB.



Texas Instruments
TI TPD4EUSB30 ESD Suppressors

• 4-channel protection for
  USB 3.0 interfaces
• Low capacitance 0.05pF
  (IO to IO)
• Space saving DQA
  (1mm x 2.5mm) package

Amphenol
Amphenol GSB3 Series USB 3.0 Connectors

• USB 3.0 enables
  5Gb/s data rates
• A, B, and Micro-B type
  receptacles and plugs
• Backwards compatible
  with Hi-Speed USB 2.0

Wurth Electronics
E-CNSW High Frequency Common Mode Line Filters

• High CMR suppression at
  high frequencies
• Winding symmetry
  ensures minimum
  signal distortion
• Reflow solderable 0603
  and 0805 package
  options

NXP
NXP PTN36241B USB 3.0 Re-Drivers

• Dual-channel USB 3.0,
  supports 5Gbps per
  channel
• I²C-bus MUXing & 5-level
  logic configuration options
• Selectable transmit
  de-emphasis & output
  swing
Featured Articles
As innovation continues to advance, large inexpensive storage, media formats, and new devices are converging. Answering the need for more bandwidth to maintain the interactive experience users expect, USB 3.0 delivers a new standard. USB 3.0's SuperSpeed data communication rate, optimized power efficiency, simplicity and ubiquity are unrivaled.
Contributed by Cypress
Architecture, power management, and a new streaming data model are some of the considerations with the update to SuperSpeed. Compare USB 3.0 with other interfaces, plug-and-play, hot swap, speed, efficiency and other attributes that change the way the game is played.

Contributed by TI
Ever wonder why the standards body did what they did? What's that bump on the B-connector for? Efficiency, standards for charging devices, the truth about backward compatibility, and the mysteries of old and new connectors are discussed here.
Contributed by Littelfuse
SuperSpeed introduces faster transfer rates, which means higher frequencies. With higher frequencies comes greater complexity in selecting the right protection. The introduction of additional differential data pairs requires more data lines to be protected against ESD than USB 2.0.