|    Change Country Change Location USD
 
United States United States

Please confirm your currency selection:

US Dollars
Home » Applications & Technologies » Industrial Application - Programmable Logic Controller
Applications & Technologies

Industrial Application - Programmable Logic Controller

A programmable logic controller (PLC) is an electronic device used in many industries to monitor and control building systems and production processes. Unlike PCs and smartphones, which are designed to perform any number of roles, a PLC is designed to perform a single set of tasks, except under real-time constraints and with superior reliability and performance.

To meet the demands of harsh industrial environments, PLCs are designed to be extremely robust, often capable of withstanding extreme temperatures, humidity, vibration, and electrical noise. Logic controllers are commonly tasked with monitoring and controlling a very large number of sensors and actuators, and are therefore distinct from other computer systems in their extensive input/output (I/O) arrangements.

VREF
Air Flow
Sensor
Temperature
Sensor
Position
Sensor
Liquid Level
Sensor
Limit Switch
Vibration
Sensor
VREG
Amp   
Amp   
Amp   
Amp   
Serializer
Serializer
Serializer
PMIC
Real Time
Clock
   ADC
   ADC
   ADC
Processor
Digital
Isolation
VREF
DAC   
Driver
ZigBee
Module
RS-232
Transceiver
CAN
Transceiver
Ethernet
Transceiver
Amp   
Amp   
Relay
ESD
ESD
ESD
D-Sub
Circular Metric
Connectors
RJ-45

This design is for reference only. The design, as well as the products suggested, has not been tested for compatibility or interoperability.

Reference Voltage ICs for PLCs

A voltage reference produces a constant level of voltage over time regardless of load, changes in power supply, or temperature. Voltage references are used in power supplies, analog-to-digital converters, digital-to-analog converters, and many other applications where voltage levels must be maintained at a steady level. Without a voltage reference, precision is greatly affected and may render the device inoperable. Voltage references can vary greatly in performance. A voltage reference for a power supply might hold its output to within only a few percentage points off of its nominal or stated value; however, a voltage reference to instrumentation-level standards are measured in parts per million regarding stability and precision to the nominal or specified value.

» View All Featured Reference Voltage ICs for PLCs

Featured Suppliers

Air Flow Sensors for PLCs

Air flow sensors are devices that measure the volume or mass of air passing through a given area per unit time. One of the most common of these sensors measure air flow using thermal-based sensing. Greater air flow causes faster cooling of a thin wire or film which is heated above the ambient air temperature. As air flow increases, more current must be passed through the heated object to maintain a constant temperature. Together with a bridge circuit and thermistor (to compensate for variations in air temperature), the sensor is capable of measuring air flow with high precision and fast response time.

» View All Featured Air Flow Sensors for PLCs

Featured Suppliers

Temperature Sensors for PLCs

A temperature sensor is a device that measures cold or heat as a temperature or temperature gradient. Many applications require some implementation of temperature sensing and measurement. For motors, the operating temperature inside the case is monitored by the processor and set to alarm or shut down at temperatures higher than the normal operating temperature of the motor. If a motor runs at too high of a temperature for too long, it can reduce the life of the motor. Operating temperature is an indication of the general operating health of the motor. Higher temperatures inside the motor case can mean too high of a load is placed on the motor, since as load increases, motor current consumption increases to meet the load requirements.

» View All Featured Temperature Sensors for PLCs

Featured Suppliers

Position Sensors for PLCs

A position sensor is any device that permits position measurement. It can either be an absolute position sensor or a relative one. Position sensors can be either linear or angular.

Poisitioning Sensors are finding their way into more handheld, Industrial Applications and industrial devices every day. Knowing the position and orientaion of a device or tool is critical for any modern control system to work accurately. Examples are as varied as a smart phone, a drilling platform, or the attitude control of a Boeing 777.

» View All Featured Position Sensors for PLCs

Featured Suppliers

Liquid Level Sensors for PLCs

A liquid level sensor is used to detect the fluid level in a container. Although some types of level sensors can provide continuous measurements, point-level detectors are generally used for applications in which only a small number of threshold levels (e.g., a maximum and minimum) need to be monitored. Sensing methods are wide and varied, with the primary criterion for selection being the specific application for which a sensor is needed.

» View All Featured Liquid Level Sensors for PLCs

Featured Suppliers

Limit Switch for Programmable Logic Controllers

An electrical switch is a device that can close and open a circuit. Limit switches are, in general, electromechanical devices and are operated by the motion of some external object such as a machine part. In an HVAC system, a limit switch is often used to monitoring the state of a damper or valve.

» View All Featured Limit Switch for Programmable Logic Controllers

Featured Suppliers

Vibration Sensors for PLCs

Vibrations produced by industrial machinery often serve as an indicator of that machine’s state of repair. Continuing to operate equipment that is already in need of servicing can exacerbate the damage or even destroy the machine. Vibration sensors provide a means for rapidly disabling a malfunctioning machine to prevent further damage, and can in many cases predict the malfunction before it even occurs. In an HVAC system, the electric motor(s) may include vibration sensors as an added precaution against mechanical and electrical defects.

» View All Featured Vibration Sensors for PLCs

Featured Suppliers

Voltage Regulators for PLCs

DC/DC regulators are circuits that convert DC voltage from one level to another and maintain that voltage to a constant level. Electronic systems often have several sub-circuits, each with its own voltage level requirement that may be higher or lower than the main power supply. Step-up converters or regulators boost a voltage to a higher level. Step-down converters or regulators lower (or B74“buck”) a voltage to a lower level. DC/DC converters and controllers can also be used for the same purpose, but may offer options such as multiple softstart levels, undervoltage lockout, protection against overvoltage and undervoltage, and programmable short-circuit protection. All of these devices are considered to be in the same category of integrated chips, typically categorized as power management devices.

» View All Voltage Regulators for PLCs

Featured Suppliers

Precision Amplifiers for PLCs

A precision amplifier is used for sensors to preserve accuracy. It increases the amplitude of weak signals it receives while introducing as little noise as possible so that the signal transfers an accurate or precise measure of what it is sensing. Amplifiers have enormous voltage gain, often use feedback of the output signal back to the input of the amplifier to operate, and can be classified in different ways. An amplifier can be identified by the device they are intended to drive (e.g., audio amplifier), the input that they are to amplify (e.g. sensing amplifier), the frequency range of the signal (e.g., RF, audio), and by the function that they perform (e.g. buffer amplifier, current-sensing amplifier.)

» View All Precision Amplifiers for PLCs

Featured Suppliers

Instrumentation Amplifiers for PLCs

Amplifiers have enormous voltage gain, use feedback to operate, and can be classified in different ways. They can be identified by the device they are intended to drive (e.g., headphone amplifier, speaker amplifier), the input that they are to amplify (e.g. guitar amplifier), the frequency range of the signal (e.g., RF, Audio), and by the function that they perform (e.g. inverting amplifier, power amplifier.)

» View All Instrumentation Amplifiers for PLCs

Featured Suppliers

Serializers for PLCs

A serializer is a transceiver that converts multiple streams of parallel data into a single serial data stream. These devices are used to compensate for limited I/O. They and are often coupled with a deserializer and called a SerDes (serializer/deserializer), and are used to reduce the number of required inputs and/or outputs.

» View All Serializers for PLCs

Featured Suppliers

Power Management for PLCs

A Power Management Integrated Circuit (PMIC) is a special-purpose IC that provides one or more power management related functions. These can include voltage regulation, DC/DC conversion, battery management capability and more. Many PMICs offer an I2C and/or SPI bus interface, and some might provide additional features such as an integrated touch screen interface.

» View All Power Management for PLCs

Featured Suppliers

Real Time Clocks for PLCs

Real Time Clocks (RTCs) are IC devices that keep track of time. A typical RTC can provide the time of day as well as the date via a serial bus such as I2C or SPI. Although similar in many ways, RTCs should not be confused with clock generators, which are used to synchronize various parts of a circuit.

» View All Real Time Clocks for PLCs

Featured Suppliers

Analog-to-Digital Converters for PLCs

An Analog-to-Digital Converter (ADC or A/D converter) measures the magnitude of an input analog signal and converts it to a digital number that is proportional to the magnitude of the voltage or current. An ADC often converts signals collected from the real-world to digital signals for processing. One of the more important specifications of an ADC is the resolution that it offers, which is the number of discrete values (represented in bits) that the ADC produces in relation to the analog signal it is converting. The more bits, the higher the resolution. A higher resolution yields a more accurate approximation of the analog input.

» View All Analog-to-Digital Converters for PLCs

Featured Suppliers

Processors for PLCs

The term "processor" refers to an electronic device that performs computational functions and carries out the instructions of a stored program. Other terms for processor are microprocessor, central processing unit, and digital signal processor. Essentially, the processor refers to "the brains of a computer."

» View All Processors for PLCs

Featured Suppliers

Digital Isolation for PLCs

Isolation is critical to protect both an electronics system and the user from potentially hazardous voltages, or where a high level of electrical isolation between electronics systems is necessary. Considerations for digital isolators are speed of data transmission, high level of magnetic immunity, and long life expectancy. Used in combination with isolated power supplies, these devices block high voltages, isolate grounds and prevent noise currents from entering the local ground and interfering with or damaging sensitive circuitry. Digital isolators can be used to implement isolation in designs without the cost, size, power, performance, and reliability constraints found with optocouplers.

» View All Digital Isolation for PLCs

Featured Suppliers

Digital-to-Analog Converter for PLCs

A digital-to-analog converter (DAC) is a semiconductor device that is used to convert a digital code into an analog signal, such as electric charge, current, or voltage. An analog-to-digital converter (ADC) performs the reverse operation. A DAC is the principal means by which computer and digitally-based systems translate digital data into real-world signals.

» View All Digital-to-Analog Converter for PLCs

Featured Suppliers

Relay Drivers for PLCs

Designers of power electronic circuits must often drive power switches that feed DC, AC, or power signals to a variety of workloads. Logic-level electronic circuits provide the driving signals. In general, however, the power sources and their loads have reference levels different from that of the control circuitry (ground). MOSFET selection begins by choosing devices that can handle the required current, then giving careful consideration to thermal dissipation in high current applications.

» View All Relay Drivers for PLCs

Featured Suppliers

ZigBee Wireless Modules for PLCs

Zigbee is a specification for communication in wireless personal area networks (WPANs) and is designed for low-power, cost-efficient, and low duty cycle applications. Built upon the IEEE 802.15.4 standard, Zigbee adds both routing and multi-hop functionality. Star networks as well as peer-to-peer (e.g., mesh and cluster tree) are supported, making Zigbee networks dynamic, scalable, and decentralized. These qualities and more make Zigbee an excellent technology for applications like home/industrial automation, Industrial Applications monitoring, and HVAC control.

» View All ZigBee Wireless Modules for PLCs

Featured Suppliers

RS-232 Transceivers for PLCs

RS-232 refers to a set of standards for single-ended serial communication, and covers such things as logic voltage levels, timing, signal rate, and physical characteristics of the connectors. An RS-232 port was once the standard interface for connecting a personal computer with peripherals such as keyboards and modems, but has since been largely replaced by USB. It continues to be used in other areas however; much of today’s industrial automation equipment incorporates RS-232.

» View All RS-232 Transceivers for PLCs

Featured Suppliers

CAN Transceivers for PLCs

CAN is an acronym for Controller Area Network and refers to a fault-tolerant communications protocol that is flexible for system design, supports multiple network topologies, and has become a de facto standard for high integrity serial communications in industrial and automotive embedded applications. In a CAN network, several short pieces of data like a motor’s run status, temperature, or RPM is broadcast over the entire network at up to 1 megabit per second (Mbps.) CAN is meant for applications that have to report and consume numerous but small pieces of data consistently among nodes and has the ability to self-diagnose and repair data errors. CAN is well-suited to environments with machinery, since CAN is designed to be reliable in rugged environments that include interference or introduce noise. CAN is also well-suited to the transportation industry.

» View All CAN Transceivers for PLCs

Featured Suppliers

Ethernet Transceivers for PLCs

Ethernet is the most commonly used technology for non-wireless local area networks (LANs). Ethernet controllers perform the function of interfacing computers and other electronic devices in a network. Ethernet itself only defines the physical (PHY) and datalink (MAC) layers of the OSI Model; however, processors with integrated Ethernet controllers can provide additional functions such as a TCP/IP protocol stack.

» View All Ethernet Transceivers for PLCs

Featured Suppliers

Current Driving Amplifiers for Programmable Logic Controllers

Current sensing amplifiers, also known as current-sense or current-shunt amplifiers, measure electrical current. The voltage across a resistor in a current path is directly proportional to that current, per Ohm's law. Thus, measuring current is highly dependent upon the resistor for accuracy. Integrated circuits for current measurement are more efficient, accurate, and are an overall lower cost solution over a discrete current-sense solution.

» View All Current Driving Amplifiers for Programmable Logic Controllers

Featured Suppliers

Relays for PLCs

Simply put, a relay is an electrical switch that is controlled electrically. Relays are often necessary to control high power/current/voltage circuits with a low-power signal while maintaining complete electrical isolation between them.

Many relays are electromechanical in nature; the control signal energizes an electromagnetic coil creating a magnetic field. This field exerts a force on a movable armature of ferromagnetic material (such as iron) which makes or breaks the electrical connection.

Solid State Relays (SSRs) are another common type, and unlike their electromechanical equivalent, they have no moving parts. Instead, one or more transistors, such as a MOSFET, are used to provide a similar function. Electrical isolation must be added in this case, often by using an on-chip optocoupler.

» View All Relays for PLCs

Featured Suppliers

Interface ESD for PLCs

If you have ever been zapped by a socks-wearing kid who has just discovered static charge build up, you have experienced ESD first hand. ESD is like a miniature, localized lightning bolt caused by an electrical discharge. ESD can have seriously damaging effects on an integrated chip or system, or can cause poor performance or failure later on by merely weakening the circuits.

» View All Interface ESD for PLCs

Featured Suppliers

Ethernet ESD for PLCs

Electrostatic Discharge (ESD) is a naturally occurring phenomenon. If you have ever been zapped by a socks-wearing kid who has just discovered static charge build up, you have experienced ESD first hand. ESD is like a miniature, localized lightning bolt caused by an electrical discharge. ESD can have seriously damaging effects on an integrated chip or system and cause poor performance or failure later on by merely weakening the circuits.

» View All Ethernet ESD for PLCs

D-SUB Connectors for PLCs

A D-sub or "D-Subminiature Connector"contains two or more parallel rows of pins or sockets, usually surrounded by a D-shaped metal shield that provides mechanical support, ensures correct orientation, and may screen against electromagnetic interference. The part containing pin contacts is called the male connector or plug, while that containing socket contacts is called the female connector or socket.

» View All D-SUB Connectors for PLCs

Featured Suppliers

Circular Metric Connectors for Programmable Logic Controllers

Circular Metric Connectors are cylindrical in shape and can have pin positions that make it impossible to mate in the wrong direction. This is useful for when mis-connecting equipment can be catastrophic and fault-proof connections are needed. Data rates, shielding, electrical characteristics, size, materials, and pin positions or contacts can vary widely, depending upon use. These connectors are available in several shell and termination styles.

» View All Circular Metric Connectors for Programmable Logic Controllers

RJ-45 Connectors for PLCs

RJ-45 connectors are a type of electrical connector commonly used for Ethernet jacks. The term "RJ-45" is something of a misnomer, but it almost always refers to an 8P8C (eight position, eight contact) modular connector with wiring pin-outs compatible with standard Ethernet.

» View All RJ-45 Connectors for PLCs

Featured Suppliers