Contact Mouser (USA)  (800) 346-6873     |     Feedback        
View Cart     |     Change Location  USD
United States United States

Please confirm your currency selection:

US Dollars
NEDA Authorized FTDI Distributor
FTDI
   
View all FTDI Products View FTDI NEWESTPRODUCTS

FTDI Chip develops innovative silicon solutions that enhance interaction with today's technology. Through application of its "Design Made Easy" ethos, the company is able to support engineers with highly sophisticated, feature-rich, robust and simple-to-use product platforms. FTDI Chip's long-established, continuously expanding Universal Serial Bus (USB) product line boasts universally recognized products. The company's Embedded Video Engine (EVE) graphic controllers each pack display, audio and touch functionality onto a single chip allowing dramatic reductions in the development time and bill-of-materials costs involved in Human Machine Interfaces (HMIs) implementation. FTDI Chip also provides families of highly differentiated, speed-optimised microcontrollers with augmented connectivity.

 
FTDI X-Chip Series
 
FTDI FT800 Embedded Video Engine FTDI FT311D USB Android Host ICs
 
FTDI Newest Products

FTDI New Products

Newest Products From FTDI

FTDI Featured Products

FTDI Resources & Support

 
FTDI Drivers

PLEASE NOTE - When updating drivers, refer to the following document: AN_107 - Advanced Driver Options

Drivers are available which allow FTDI devices to work with the following operating systems:

  • Windows Server 2008 R2
  • Windows 7
  • Windows 7 x64
  • Windows Server 2008
  • Windows Server 2008 x64
  • Windows Vista
  • Windows Vista x64
  • Windows Server 2003
  • Windows Server 2003 x64
  • Windows XP
  • Windows XP x64
  • Windows 2000
  • Windows ME
  • Windows 8
  • Windows 98
  • Linux
  • Mac OS X
  • Mac OS 9
  • Mac OS 8
  • Windows CE.NET (Version 4.2 and greater)

For most of these operating systems two types of driver are available: Virtual COM Port (VCP) drivers and direct (D2XX) drivers. The VCP driver emulates a standard PC serial port such that the USB device may be communicated with as a standard RS232 device. The D2XX driver allows direct access to a USB device via a DLL interface.

To locate the drivers you want to install for a device, select which of the driver types you wish to use (VCP or D2XX) and then locate the appropriate operating systems. With the exception of Windows 98 and Windows ME, all devices are supported in each driver package.

 
FTDI Firmware

The FTDI firmware section includes firmware development tools and resources for the FTDI Vinculum USB Host / Slave controller devices. The section is divided into tools for the VNC2, containing Vinculum-II Development Tool Suite with latest tool releases and application examples. The Vinculum section lists application examples and utilities for the VNC1L, while the precompiled f/ware section contains precompiled firmware images for both the VNC1L and VNC2.

  • Vinculum-II Tools

    Development tools and utilities to aid application development on the Vinculum family of USB Host/Slave controller products.

  • Vinculum Tools

    Sample applications and utilities designed for use with the first generation Vinculum VNC1L USB Host / Slave controller.

  • Precompiled Firmware

    Downloads featuring FTDI's pre-compiled firmwares for the Vinculum VNC1L and VNC2 USB Host / Slave controllers. The firmware files provide a ready-to-use application firmwares for the Vinculum devices with integrated USB class drivers for a range of applications including USB disk interfacing, HID (Human Interface Devices), HUBs and communication class devices (CDC).

FTDI Videos