CURRENT REGULATOR DIODES 781-J500-E3, 781-J501-E3, 781-J502-E3, 781-J503-E3, 781-J504-E3, 781-J505-E3, 781-J506-E3, 781-J507-E3, 781-J508-E3, 781-J510-E3, 781-J511-E3, 781-SST502-E3,781-SST502-T1-E3,781-SST503-E3, 781-SST503-T1-E3, 781-SST504-E3, 781-SST504-T1-E3, 781-SST505-E3, 781-SST505-T1-E3, 781-SST506-E3, 781-SST506-T1-E3, 781-SST507-E3, 781-SST507-T1-E3, 781-SST508-E3, 781-SST508-T1-E3, 781-SST509-E3, 781-SST509-T1-E3, 781-SST510-E3, 781-SST510-T1-E3, and 781-SST511-T1-E3 In late 1999, Siliconix closed the wafer fabrication plant in Santa Clara, which had been their source for JFET wafers for many years. They then contracted with a foundry for continued supply. In 2005, their foundry source announced the closure of the line supporting JFET demand, and they placed and completed a lifetime buy for these devices. They are currently in the process of finding a new source, and expect that to be completed and on line in the second half of 2007. In the meantime, Vishay-Siliconix can support JFET demand only from their existing inventory of wafers. They cannot add to that inventory. Typically, a given JFET die type yields to a number of JFET part-types. Depending on the parts needed, the wafer lot must be targeted so that the yield is optimized to support the parameters needed. If wafers in stock are not targeted correctly, yield for a given part may be very low, meaning you can have the right die type, but not be able to yield to the specific part. Since they cannot target new wafer lots to support specific parts, they are now finding that they cannot yield any good parts to specific parts in the JFET product line. And specifically for the J5xx and SST5xx N Channel Current Regulators, they find that they cannot reliably yield parts given their existing wafer inventory. For this reason, they have put this series on order hold, preventing any new orders from booking. This hold will stay in place until they have qualified a new source for wafers, and can begin targeting to yield specific parts in the range, as they have in the past. If a particular new customer need is urgent, they can evaluate their existing inventory and see if they can support it. In general, they will not be able to do so. They recommend that for the time being, customers seek alternate sourcing for this series. 5-1206-28